DA Groups

The DA Groups category provides status information about the DA Groups to which a client subscribes. Each DA Group consists of items that the client is being used to monitor, for example, values on a Mimic.

The method used to subscribe to an DA Group varies according to the client application. For ViewX, there is an DA Group per Mimic, so a Mimic that contains an embedded Mimic will subscribe to 2 DA Groups.

The status information for the DA Groups is categorized under these headings:


Disclaimer

ClearSCADA 2017 R3