Find Updates for a Specific Driver

Update information is available for many of the drivers that ClearSCADA supports. You can use the update feature to find out about, and learn how to obtain, the latest driver updates. To access the update information, your computer needs access to the Internet.

To access the Update feature:

  1. Display the Modules status information in the Server Status Window (see Modules).
  2. From the list of drivers that are installed, right-click on the driver for which you require update information.
  3. Select the Update Information option from the context-sensitive menu.
    The relevant online update information page is displayed (providing that your computer has access to the Internet).

Further Information

Get Support for a Specific Driver.

Access Documentation for a Specific Driver.


Disclaimer

ClearSCADA 2017 R3