Server Status Information

The Server Status Tool provides status information that is organized into groups of categories, each of which contains sub-categories. The Server group provides status information about the server on which you are using the Server Status Tool and it contains the following sub-categories:


Disclaimer

ClearSCADA 2017 R3