Internet Explorer 11 XSS Filter Issue - ‘Hanging’

This issue only applies when using an Original WebX client, rather than a WebX client.

A bug in Internet Explorer 11 may cause ‘hanging’ - Internet Explorer will ‘freeze’ and be unable to display the requested information. This relates to a problem with Internet Explorer 11’s Cross-Site Scripting (XSS) filter and compatibility settings and only occurs if you use Original WebX to access a ClearSCADA server:

Typically, the ‘hanging’ occurs when displaying Query lists (including Events Lists) that have complex filters. For example, if you use Original WebX to display an Events List that has multiple WHERE, AND, OR filters specified in its query, Internet Explorer may ‘hang’. A common situation in which this can occur is when the Display Events action is selected for an object on a Mimic.

'Hanging' can also occur when trying to access a 'custom' Ad Hoc Trend, for example via a hyperlink on a Mimic. (A 'custom' Ad Hoc Trend is a Trend that has been defined using TrendSpec, ClearSCADA's specification language.)

There are two simple and effective work arounds that will allow you to display filtered query lists and Ad Hoc Trends in Original WebX.

Either:

Or:


Disclaimer

ClearSCADA 2017 R3