Operational Limitations - Client

ClearSCADA has a number of recommended operational limits. Expansion beyond the recommended limits is possible, but may result in a system that is unstable and unreliable. The recommended operational limits for ClearSCADA clients are:

Parameter

32-Bit Limit

64-Bit Limit

Notes

Minimum ViewX to ClearSCADA server link bandwidth

2 Mbit

2 Mbit

Exceeding these limits will cause slow performance in ViewX.

Maximum ViewX to ClearSCADA server link latency

150 ms

150 ms

Exceeding these limits will cause slow performance in ViewX.

Minimum WebX client to WebX server link bandwidth

1 Mbit

1 Mbit

 
Minimum Original WebX client to ClearSCADA server link bandwidth

1 Mbit

1 Mbit

 

For information on server operational limitations, please see Operational Limitations - Server.


Disclaimer

ClearSCADA 2017 R3