Example Configuration

The topics in this section include several examples to demonstrate how TrendSpec can be used to allow users to view data in Trend form. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

Remember that if scripting is to be used on a Mimic, you must first enable the scripting feature on that Mimic (see Enable the Scripting Feature on a Mimic).

For further information on scripting, see the ClearSCADA Guide to Scripting.


Disclaimer

ClearSCADA 2017 R3