View Earlier or Later Values on a Trend

When you display a Trend, it shows a specific amount of time on the X-Axis. This amount of time is defined in the configuration of the Trend and is called the interval. You can set the Trend to display data for a different interval. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

Also see:


Disclaimer

ClearSCADA 2017 R3