Edit Tab

The Edit tab appears on the ViewX Ribbon. It contains the following command groups:

The Save, Clipboard and Undo /Redo groups include commands that mainly apply to users with higher security permissions. The exception to this is the 'Save in Document Store' command, which you can use to Add a Copy of a Document to your Operator Document Store.

The Design group includes the Design Mode command, used by high-level users to switch between Run Mode and Design Mode while configuring database items.


Disclaimer

ClearSCADA 2017 R3