Document Display Area Database Bar ViewX Ribbon Home Tab

The ViewX Window

When you run ViewX, the window typically contains the following components:

The Alarm Banner informs you about any existing or recent alarms on the system. You navigate the system using the ViewX ribbon and Explorer Bar. You view the displays you require in the document display area. The Status Bar provides information on the status of the system and user activity.

For more information on these components, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

ClearSCADA 2017 R3