Use Custom Hyperlinks on a Mimic on a WebX Client
            Your system may include Mimics that have been configured with custom hyperlinks that, when selected, either:
- Replace the existing display with that of another display, such as another Mimic, Trend, or List
 
or:
- Display a ‘custom’ pick action menu that provides access to other items, displays and/or options.
 
Example:
A pump on a Mimic is configured to display a ‘custom’ pick action menu.
A user selects the pump on the Mimic. The ‘custom’ pick action menu is displayed.
                        
                    
The user selects the required option. In this particular case, the Display Faceplate option.
The current Mimic display is replaced with one that shows specific status information about the database item, similar to that shown in ‘standard’ Status Displays.
                        
                    
For more information on custom hyperlinks, see the ClearSCADA Guide to Mimics.