Reset the Zoom Level

You can Zoom In or Out and Pan Along the X-Axis on an X-Y-Z Plot. To return the x-axis to show its full span, you reset its zoom level. To do this:

  1. Right-click on the x-axis.
    A context-sensitive menu is displayed.
  2. Select the Zoom option.
    A further context-sensitive menu is displayed.
  3. Select the Reset Zoom option.
    The x-axis zoom level reverts back to show the full range that is defined for that axis.

Disclaimer

ClearSCADA 2017 R3