Changing the Update Interval for a Ladder Diagram

You can use the Update Interval feature to define how often your ClearSCADA client PC requests updates for a Ladder Diagram. By default, ClearSCADA clients request an update from a ClearSCADA server for the latest variable values every second.

By using the Update Interval feature, you can set your ClearSCADA client PC to request variable updates at a slower rate.

To change the update interval for a Ladder Diagram:

  1. Display the Ladder Diagram in Run mode (see Display a Logic Program in Run Mode).
  2. Select the Logic tab on the ViewX ribbon.
  3. Select Update Interval in the View command group.
    A further menu is displayed.

  4. Select the required interval from the list of options. The intervals range from 1 second to 60 seconds.

Disclaimer

ClearSCADA 2017 R3