Enable Execution
            Associated with: ST Programs, Function Block Diagrams, Ladder Diagrams, Sequential Function Charts
Security permission required to access this pick action: Configure
By using the Enable Execution action, you can allow a Logic program to be executed via the Execute action or Execute method. The Enable Execution action is only available on Logic programs that currently cannot be executed (programs that previously had their Disable Execution action selected).
You can see whether a Logic program has had its execution status set to enabled or disabled by using the Status Display (the Execution status shows Enabled or Disabled). For more information, see Logic Specific Status Attributes.