Enable or Disable a Logic Program
            ClearSCADA can only execute active Logic programs. Logic programs are active by default, but they can be deactivated (and re-activated) by selecting the In Service check box on the Logic tab.
To enable or disable a Logic program:
- Display the configuration Form for the relevant program (see Configure an ST Program, Ladder Diagram, SFC or FBD).
 - Select the Logic tab.
 - Check the In Service check box to enable the program or clear it to disable the program.
 
To configure the other Logic tab settings, see Configure an ST Program, Ladder Diagram, SFC or FBD.