Choose a Type of Alarm Redirection

There are several types of alarm redirection. Choose the type of redirection suitable for your system and the item that you are configuring. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

You can also configure any of the redirections to run on a roster basis, with different redirections triggering in a different order on different days (see Action Roster), or on a calendar basis, allowing you to readily set up redirections for different types of day (non-working, public holiday, and so on) (see Alarm Redirection Calendar).


Disclaimer

Geo SCADA Expert 2019