Test Your Knowledge on the Virtual ViewX Interface

How much do you know about the Virtual ViewX interface? Try and answer the following questions:

  1. Virtual ViewX is designed to allow remote access, but can it be used to access your system from anywhere?
  2. Apart from remote access and appearance, what is the main difference between Virtual ViewX and ViewX?
  3. What features are used to help prevent unauthorized access via a Virtual ViewX client?
  4. How do you access Virtual ViewX?
  5. If you don’t have a mouse with a wheel, how can you zoom in on a Mimic in Virtual ViewX?
  6. You can use your web browser’s Back and Forward buttons to navigate through Virtual ViewX displays in the order in which you originally displayed them. But what other ways are there of accessing different Virtual ViewX displays?
  7. You want to display status information about a specific point. How might you do this in Virtual ViewX?
  8. You are logged on via a Virtual ViewX client when an alarm is raised. You are responsible for responding to the alarm, so what do you do?
  9. How can you filter the Alarms List so that it only displays alarms that relate to items in a specific Group?
  10. You display the Events List and its entries are sorted in Time order. You want them to be sorted according to their Severity and so create a new Severity sort method. You apply the Severity method but the Events List still appears to be sorted according to time. Do you know why?
  11. You want to perform a Hand Control on a database point via Virtual ViewX. How would you achieve this?
  12. The Alarm Banner contains an alarm that is associated with a database item. You want to locate that database item in the database. How would you do this?

Disclaimer

Geo SCADA Expert 2019