Clear Data
Associated with: Dynacard Stores
Security permission required to access this pick action: Diagnostics
LOSS OF DYNACARD DATA
Use the Clear Data pick action with care. Once triggered, the pick action will permanently delete the sets of dynacard data that are stored in Geo SCADA Expert for the selected Dynacard Store.
Use the Clear Data pick action to permanently clear the existing sets of dynacard data from a Dynacard Store (including Stored, Shutdown, and Malfunction dynacard data). Use the pick action, for example, if the existing sets of dynacard data are corrupt or inaccurate.
There is no need to use this pick action during normal operation. Geo SCADA Expert discards the oldest sets of dynacard data automatically whenever it uploads further sets of dynacard data, as defined by the storage limits that are specified for the Dynacard Store (see Configure the Dynacard Storage Properties).
(To delete or replace just the existing set of 'Reference' data, use the Delete Reference Dynacard Data or Copy a Stored Card to Reference Card pick actions instead.)