Configure the Properties on the Dynagraph Form
To configure the properties on the Dynagraph Form, you need to display the Form (see Display a Form).
The Dynagraph Form has these tabs:
Use to configure the Identification properties (see Defining Identification Details).
Use to specify the item's geographical coordinates. (You need only configure the properties on this tab if your system uses Geo SCADA Expert's Geographical Location features.)
Use to define any custom pick actions (‘methods’) for the Dynagraph (see Using the User Methods Tab to Define Custom Actions]).