Show or Hide the Grid Lines
You can optionally display grid lines on an x-axis or a y-axis. The grid lines are a visual indicator that can make it easier to determine the values shown on the Dynagraph.
To display or hide the grid lines:
- Display the Dynagraph in Run or Design mode, as required (see Displaying an Editor).
- Right-click on the x-axis or y-axis, as required.
A context sensitive menu is displayed. - Either:
- Select the Show Grid option so that it is prefixed by a check mark.
The relevant grid line is displayed (a vertical line for the x-axis, or a horizontal line for the y-axis). - Clear the Show Grid option so that the check mark is removed.
The relevant grid line is hidden from display.
- Select the Show Grid option so that it is prefixed by a check mark.