Remove an Extra Alarm Column

You can use the Extra Alarm Columns window to remove any of the extra alarm columns from the Alarms Lists and Alarm Banner.

To remove an extra column:

  1. Display the Extra Alarm Columns Window.
  2. Select the name of the column that you want to remove.
  3. Select the Remove button to delete the extra alarm column.
  4. Select the OK button to confirm your selection(s) and close the Extra Alarm Columns window.
    The column is removed from the Alarm Banner on ViewX clients, and from Alarms Lists when they are next displayed. If a user is logged on to a Virtual ViewX client when the changes are implemented, they will have to log off and then back on to that client in order for the Alarm Banner to omit the removed column.

Disclaimer

Geo SCADA Expert 2020