Remove the Alarm Banner
The Alarm Banner is displayed on most ViewX and Virtual ViewX clients by default. Although we do not recommend it (as you may not become aware of new alarms on the system), you might want to remove the Alarm Banner so that it is not on display.
You can only remove the Alarm Banner if your User Account has the Can Remove Banner feature enabled.
LACK OF AUDIBLE ALARM NOTIFICATION
To remove the Alarm Banner on a ViewX client or Virtual ViewX client:
- Display the Home tab on the ViewX ribbon.
- Deselect Alarm Banner in the Operate command group.
The Alarm Banner is removed.