Failed Third-Party OLEDB Client - System Connections

If the OLEDB client - system connection cannot be established, the OLEDB client will be unable to connect to Geo SCADA Expert.

The connections will fail to establish if:

The firewall rules for third-party OLEDB client - system connections are the same as those for ViewX - system connections.

Further Information

Firewall Settings for Client - System and Server Advise Connections.

Understanding Client - System and Server Advise Connections.

Certificates for Geo SCADA Expert Server and Client Connections.

Use the Server Status Tool to ascertain the current status of server - client connections: see Server Status Information.

 


Disclaimer

Geo SCADA Expert 2020