Bad Quality Alarm Disabled Control Disabled Point Action Future Data

Priority of Point Foreground Colors

This chart indicates which point status takes precedence over another, and therefore which core system foreground color is assigned to a point at any particular time:

As such, if an output point:

the point’s foreground color will be an orange-red, by default, to indicate that controls are disabled on that point (unless a driver-specific state applies, which takes priority over the Control Disabled state).

Further Information

List of Core System Colors.

Alarm and Event Severities.

see Defining a Custom State Color.


Disclaimer

Geo SCADA Expert 2020