Comms Lost
Associated with: Historic List entries for DNP3 Points that have Historic enabled.
The Comms Lost status is indicated by a light blue foreground color, by default.
This color is used in the Historic List to indicate that communications have been lost with the DNP3 outstation on which the point is located.
With some types of DNP3 outstation, Geo SCADA Expert can detect whether the connection between that DNP3 outstation and any remote device to which it is connected has been lost. In such a situation, only the points on the remote device are assigned the Comms Lost status.