Execute Command
Associated with: DNP3 SCADAPack E outstations and DNP3 SCADAPack Remote E outstations
Security permission required to access this pick action: Retrieve Data
Use the Execute Command pick action to execute a particular command. This section details only commands that are specific to DNP3 SCADAPack E Outstations. For further information on using the Execute Command action, see Execute Command in the Geo SCADA Expert Guide to the DNP3 Driver.
SCADAPack E outstations support the execution of a number of commands via DNP3 including:
- APPEND—Append a file to the end of another
- CLEAR—Clear specified PDS information
- COPY—Duplicate a file
- DEL—Delete a file
- RENAME—Rename a file
- RESTART—Restart PDS facilities
- FILEDIAG—Log diagnostics to a file.
For further information on using these commands on SCADAPack E outstations via DNP3, see the SCADAPack E Operation Reference Manual.