Status Attributes Associated with Channels on Simple Drivers
The channels on simple drivers support a combination of these status attributes:
- Id
- Full Name
- Type
- Position
- Created—(New channels only)
- Last Modified
- Configuration Change CRC—(Only displayed if this feature is enabled on your system)
- Exclusive Control User—(Only channels that are under Exclusive Control)
- Alarm State
- Alarm Last Updated
- State Alarm
- Alarm Count
- Source
- State
- Last Updated
- Quality
- Comms Logging
- Telnet.
For information on channel status attributes that are not listed above, see the driver-specific documentation.