Configuration Group

Each Run0x group in the FloBossDemo.sde contains a Configuration group.

The Configuration group contains points to read the orifice plate diameter and pipe diameter. Both of these points have their Control aggregate enabled, so that their values can be changed.

The group also contains a MeterConfigurationOptions point, which reads a bitfield (BIN) value from the FloBoss. The second bit of this bitfield value is used to indicate the tap location for the run. The tap location is decoded as a string on the Configuration Mimic (this is done without using script, by writing an expression to read the point’s CurrentValueAsBoolArray tag).

The Configuration group also contains a GasComposition subgroup. The GasComposition group contains points to get the gas composition values for the meter run.

Each of the points in the Configuration and GasComposition groups are attached to the ScannerConfig scanner.


Disclaimer

Geo SCADA Expert 2020