FloBoss Scanner

The FloBoss Scanner object is one of the main configuration objects of the FloBoss Driver. This object’s configuration controls everything from whether to set the clock in the FloBoss to the scan rate for attached points.

As part of the requirements for a FloBoss Scanner to be active, it needs to a reference to a FloBoss Channel. The Scanner object is itself referenced by FloBoss Point objects.

For information about the object’s configuration and setup, see the following sections:


Disclaimer

Geo SCADA Expert 2020