How can I change the orifice plate diameter for a flow run?
To read the orifice plate diameter, set up a FloBoss Numeric Point to read from Type = 46, Location = Run number – 1 and Parameter = 10. Enable the Control aggregate on the point. To change the value, call the Control method on the Control aggregate for the point.
For further information, (see FloBoss Numeric Point).