Source

Associated with: IEC 60870-5 Slave Outstations

The Source attribute is common to many Status displays. The attribute indicates the location at which the item resides. The information shown varies, depending on the item.

The Source attribute displays the value Undefined if the item’s configuration is incomplete, in so far as the device with which the item is associated has not yet been specified.

For IEC 60870-5 slave outstations, information is displayed in this format:

Link <Link Address>:Common <Common Address>

Example:

Link 64:Common 53
(For a slave outstation that has a Link Address of 64 and a Common Address of 53.)


Disclaimer

Geo SCADA Expert 2020