User-Specific Events List Preferences
This section summarizes those Events List options that a system administrator can configure on a per-user basis. The options apply to users that log onto the system using a User Account.
The options for each individual User Account, if they are to differ from the defaults, should be specified when the User Account is added to the system.
For a user that logs onto the system using an individual User Account, use that user’s User Form to:
- Specify the default Event List Range. This defines the time period for which events are initially displayed on the Events List.
- If the Area of Interest feature is used on your system, specify any Area of Interest Filters associated with the user. This can affect which events are visible to the user.
- Specify Operational features, including whether the user actually has access to Events Lists.
For information on configuring any of the above, see Creating a User Account in the Geo SCADA Expert Guide to Security.