Add, Edit, and Remove Views on a Mimic

You can use the Views button on the Mimic Properties window to access the Views window for a Mimic. The Views button is only available when you display the Mimic Properties window for an individual Mimic (rather than via the Options window). For more information on the Views window, see Views.

Further Information

Defining the Default Mimic Properties for a Specific Mimic.


Disclaimer

Geo SCADA Expert 2020