Simple Modbus Channel Status Attributes
These status attributes are specific to channels on the Simple Modbus driver:
Two further status attributes, Primary Eavesdrop Tx Assign, and Secondary Eavesdrop Tx Assign are not used by the Simple Modbus driver.