AlarmsAndEvents Group

The ROC PlusDemo.sde file includes an AlarmsAndEvents group.

 

The group contains the Data Tables to hold events and alarms from the ROC. These are the tables that are referenced on the Scanner tab of the ScannerDaily object. If you manually create your own Data Tables to hold events or alarms, as opposed to having the driver do it for you automatically, you can optionally use the schema from these data tables as a starting point.

The Logic subgroup contains some very simple scripts that can be used to manipulate the contents of the Data Tables. These scripts are called from pick actions on the EventsAndAlarms Mimic.

Further Information

Event Data Table

Alarm Data Table.


Disclaimer

Geo SCADA Expert 2020