How long does the driver hold a TCP/IP connection open?
The driver task will hold a TCP/IP connection to a ROC open for the number of seconds specified in the TcpConnectionTimeout field on the ROC Plus Channel object. Any communication with a ROC over an existing socket, including demand polls and control requests, cause the timeout to be reset.
For further information, see ROC Plus Channel.