Is the Time Zone setting on the ROC Plus Scanner applied to non-historical data?

The ROC Time Zone setting on a ROC Plus Scanner is applied to historical data only. This is because historical data is read from the ROC with a timestamp that can be fixed and then entered into the historical record.

Current data is entered into the database with the current time.


Disclaimer

Geo SCADA Expert 2020