ROC Plus Scanner

The ROC Plus Scanner object is one of the main configuration objects of the ROC Plus Driver. This object’s configuration controls everything from whether to set the clock in the ROC to the scan rate for attached points.

As part of the requirements for a ROC Plus Scanner to be active, it needs to a reference to a ROC Plus Channel. The Scanner object is itself referenced by ROC Plus Point objects.

For information about the object’s configuration and setup, see the following sections:


Disclaimer

Geo SCADA Expert 2020