Flow Time This Month

Associated with: Flow runs

This attribute indicates the amount of time that the Flow Run has run and calculated gas flow data so far, this month. The attribute is displayed once the server has retrieved Flow Run data from a Realflo-enabled SCADAPack controller.

Example:

1W6H31M5.562S
(for a Flow Run that has been running for 1 week, 6 hours, 31 minutes, and 5.562 seconds this month)


Disclaimer

Geo SCADA Expert 2020