Uncorrected Flow Volume Last Month
Associated with: Flow runs
This attribute indicates the total uncorrected gas flow volume that the Flow Run calculated last month. The attribute is displayed once the server has retrieved Flow Run data from a Realflo-enabled SCADAPack controller, if that Flow Run performs AGA-7 Flow Calculations. The units that apply to the attribute depend on the Measurement Units system being used for the Flow Run’s Contract Units.
Example:
22.311
(for uncorrected gas flow volume in E3m3 (or 103m3))