SCADAPack x70

Create a Direct Outstation

Add a SCADAPack x70 DNP3 Direct Outstation to the database. This type of database item is available from the DNP3 sub-branch within the SCADAPack x70 branch of the Create New menu. The sub-branch corresponds to the communications protocol that Geo SCADA Expert is to use to communicate with the SCADAPack 575.

When you create the outstation, you can leave most of the configuration fields at their default values. For this tutorial, the only fields that you need to change on the outstation's configuration Form are as follows:

On the Network tab:

On the SCADAPack x70 tab:

On the DNP3 tab:

As we will be using unsolicited messages to transmit event data for this tutorial, we can leave the Class Polling and Event Scanning sections of properties at their defaults. (If we were not using unsolicited functionality, we would enable Class 1 polling, and set the Analog Input Events Scan Group and Analog Output Events Scan Group to Group 1.)

On the Outstation tab:

Once you have configured the outstation, you can proceed to Create an Analog Configuration Item.

Further Information

For further information about configuring a SCADAPack x70 DNP3 Outstation, see Configure SCADAPack x70 DNP3 Outstations.


Disclaimer

Geo SCADA Expert 2020