Create a Mimic to Display the Points
- Create a new Mimic.
-
Drag-and-drop the SCADAPack x70 DNP3 Analog Output Point onto the Mimic.
A context-sensitive menu is displayed. -
Select the Value option.
A further menu is displayed. - Select Formatted Value option.
-
Drag-and-drop the SCADAPack x70 DNP3 Analog Input Point onto the Mimic.
A context-sensitive menu is displayed. -
Select the Value option.
A further menu is displayed. - Select Formatted Value option.
- Save the Mimic.
- Put the Mimic into Run mode.
Once you have configured the Mimic, you can Download Configuration to the SCADAPack 575 Device.
Further Information
Working with Mimics: see the Geo SCADA Expert Guide to Mimics.