Define the Modbus Slave Device
When you create a Modbus Point Scanner you need to associate it with a Modbus Slave Device configuration item.
This allows you to select the Modbus Slave Device that the point scanner is associated with.
Use the browse button to display a Reference browse window and then select the required entry from the window.