SCADAPack x70

Display Devices

Associated with: SCADAPack x70 Firmware Image items

Security permission required to access this pick action: Read

Use this pick action to display a Queries List of the SCADAPack x70 Device Configuration items with which the selected Firmware Image database item is associated. The List indicates the devices on which the operating system firmware can be updated using the .biz file that was last uploaded into Geo SCADA Expert using this particular Firmware Image item.

The Display Devices pick action is not a method and therefore cannot be used with the automation interface.


Disclaimer

Geo SCADA Expert 2020