Editbox.ShowKeypad

The EditBox Control Object that is returned by the AddEditBox function has a ShowKeypad property. The Showkeypad property determines whether an alphanumeric keyboard is made available for the Edit Box. The keyboard is an on-screen keyboard display.

When the keyboard is shown, users can use it to enter numbers and letters in fields and so on, instead of using a traditional mouse and keyboard.

There are two types of on-screen keyboard:

Syntax

ControlObject.ShowKeypad = Value

Where ControlObject. is the name of the variable (declared in your script) that is used to store the EditBox Control Object that is returned by the AddEditBox function.

Description

Provides access to an on-screen keyboard for manual entry of values.

Arguments

Value {Boolean}

If set to True (1), the Edit box provides access to a keyboard; if set to False (0) the EditBox does not provide access to a keyboard and any user-defined inputs have to be made manually.

Returns

Boolean

Example:

EditBox1.ShowKeypad = 1

Where:

  • EditBox1 is the name of the variable that stores the EditBox Control Object returned by the AddEditBox function
  • 1 sets the Edit Box to have an alphanumeric keyboard.


Disclaimer

Geo SCADA Expert 2020