SetBusy

The SetBusy function allows a script to define whether the cursor changes to indicate that the script is running. This function is often used when scripts have to perform a process which can take an extended amount of time to complete—during this time, the cursor can change shape to a busy icon, indicating to the user that the script is running normally and that there is a delay before the script can run to completion.

Syntax

SetBusy (Boolean)

Description

When True, causes the cursor to indicate that a script is busy running.

Arguments

SetBusy {Boolean}

You have to set the Boolean value to True if the busy cursor is to be enabled; false if the busy cursor is to be disabled.

Returns

None. If the Boolean value is true, the cursor icon will change to indicate that a script is running; if the Boolean value is false, the cursor icon will remain the same irrespective of whether a script is running.

Example:

SetBusy (True)

The cursor icon will change when the script is running so that users can identify that the script is running and has not yet run to completion.


Disclaimer

Geo SCADA Expert 2020