Time

The Alarm.SelectedAlarms and Alarm.Alarms properties both return an alarm collection and each alarm in the collection has a Time property. The Time property represents the time at which the alarm was raised.

Syntax

Time

Description

Returns the time at which the alarm was raised.

Arguments

None.

Returns

Time {DateTime}. The time stamp for the alarm.

Example:

In this example, Alarm.Time is used to return the time stamp of the selected alarm. The time stamp is displayed in a message box next to the text "Time", and the severity description, the alarm item’s full name, and the name of the logged on user are also shown.

Function ShowAlarmInfo( Alarm )

MsgBox "One Alarm Selected", "Severity " & Alarm.SeverityDesc & ", Time " & Alarm.Time & ", logged on user name " & Alarm.Server.Username & ", Object name " & Alarm.Object.Fullname

End Function


Disclaimer

Geo SCADA Expert 2020