TopMimic Properties

The TopMimic Object has the following properties:

These properties work in the same way as the similarly named properties of the Mimic object. The only difference is that they apply to the top level Mimic (the Mimic database item that is currently displayed). For example, TopMimic.SystemName allows you to display the full name of the top-level Mimic, whereas Mimic.FullName allows you to display the full name of the Mimic that contains the script that is running. For more information on the purpose of each property, see Mimic Properties.

If the top-level Mimic is the Mimic that contains the script that is running, using the TopMimic properties will produce the same results as using the Mimic properties (as the top-level Mimic and the Mimic that contains the script are one and the same).


Disclaimer

Geo SCADA Expert 2020