Define the Type of Item with which an Extra Link Field can be Associated

When you add an extra link field, you need to specify the Target Type. This setting defines the type of item that can be selected in the link field when it is on a Form. For example, if you set the Target Type to CSCADAPackMPoint, you will only be able to use the link field to associate an item with a SCADA Pack Modbus point.

To define the target type, you need to use the Target Type setting on the Edit Field window. To access the Edit Field window, see Add or Modify an Extra Field.

When you have displayed the Edit Field window, use the Target Type setting to choose the type of database item that can be selected via the link field:

When you have defined the Target Type setting, you can continue to define the other field settings as required.


Disclaimer

Geo SCADA Expert 2020