Modify a Quality Classification
You can use the Geo SCADA Expert Server Configuration Tool to change a quality classification.
To modify a quality classification:
- Access the Geo SCADA Expert Server Configuration Tool (see Accessing the Geo SCADA Expert Server Configuration Tool).
- Expand the Database Configuration branch of the tree-structure.
- Select Quality Classifications.
- Right-click on the quality classification that you want to change.
- Select the Modify option from the context sensitive menu.
The quality description is selected so that you can alter its name. - Type in the amendments to the point quality classification, and then press the Enter key or select another part of the interface.
- Repeat steps 4 and 5 until you have modified those quality classifications that need to be changed.
- Right-click on the system icon in the tree-structure, and select the Apply Changes option to apply the changes.
Now that you have modified one or more quality classifications, you can continue with the server configuration.
If you are unfamiliar with the server configuration process, we recommend that you proceed to learn about Alarm and Event Severities.