Modify an Extra Table Query

To modify an extra table query:

  1. Access the Geo SCADA Expert Server Configuration Tool (see Accessing the Geo SCADA Expert Server Configuration Tool)
  2. Expand the Database Configuration branch.
  3. Select the Extra Table Query branch to display the Extra Table Query section.
  4. Right-click on the Extra Table Query that you want to edit.
  5. Select the Modify option.
    The Modify Query window is displayed.
  6. Use the Modify Query window to alter the configuration of the query. The Modify Query window has the same settings as the Add Query window (see Create an Extra Table Query).

Disclaimer

Geo SCADA Expert 2020